cancel
Showing results for 
Search instead for 
Did you mean: 

Passing -CP to the raisonance linker in STVD

steven239955_st
Associate II
Posted on May 23, 2012 at 16:11

The linker is not case sensitive unless the -C flag is used on the command line 

Does anyone know how to pass this flag from within ST Visual Develop?  I can't just add -C as a user flag as STVD already passes -P and to the linker and the raisonance linker only accepts -CP not -P and -C as separate arguments.  How do I replace -P with -CP in STVD?  For example, can I stop STVD passing -P so I can add the -CP flag?

If the linker is not case sensitive then the c source code needs to be written to avoid the linker seeing, for example, BOB and bob as the same symbol.  Which is giving me major code reuse problems.

#stvd-raisonance-linker
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0