2012-11-26 06:48 AM
Hello,
I am using a STM8S207K6 Microcontroller without a ST-evaluation board Compiler: Cosmic Development Tool: STVD I would like to use different moduls in my project(like UART3, TIM4 .. etc) Now, i tried to use the interrupt sources of the different modules. And i have noticed, that always the next interrupt routine in the list is called. For example(TIM4): If the interrupt bit in the Tim4_SR Register is set, the Interrupt nr. 24(EEPROM_EEC_IRQHandler) is called, and not the TIM4_UPD_OVF_IRQHandler. And i have exactly the same problem with the other modules. The Files i am using: - stm8s_it.c V2.1.0 18-November-2011 - stm8s_it.h V2.1.0 18-November-2011 - stm8s.h V2.1.0 18-November-2011 (not including the conf.h File) - stm8_interrupt_vector.c 2011 Are there any known Problems like that? Thank you! #programming-stm8s