2022-06-18 12:51 AM
Hi everyone.
I am having problem reading data on ADC pins in stm8s003k3. I have attached three NTC at Ain1/2/3(which I suppose is also known as a channel) according to the datasheet. Problem is that when I put different channels in my code it shows one reading on two displays while the third display shows a random value. Here is my code. Kindly someone guide me or a bit of a hint. Thanks
void ADC_Init (unsigned char Channel)
{
CLK->PCKENR2 |= CLK_PCKENR2_ADC;
ADC1->TDRL = Channel;
ADC1->CR1 = ADC1_PRESSEL_FCPU_D18;
ADC1->CR2 = ADC1_ALIGN_RIGHT;
ADC1->CR1 |= ADC1_CR1_ADON;
}
unsigned int ADC_Read (unsigned char Channel)
{
unsigned int Result;
ADC1->CSR = Channel;
ADC1->CR1 |= ADC1_CR1_ADON;
ADC1->CR1 |= ADC1_CR1_ADON;
while (!(ADC1->CSR & ADC1_CSR_EOC));
Result = ADC1->DRL;
Result |= ADC1->DRH << 8;
return Result;
}
2022-06-19 8:38 AM
With informations you provide one cant say more then... Probably because you are converting wrong channel. No schematic, no measured values, no complete code, no output values, no photo... i have to look for crystal ball. But one thing - why do you start conversion twice ?