2016-02-12 5:20 AM
Hello,
I want to use I2C Communication between two stm8s208cb MCUs. I use stm8s standard peripharel library. My code:Master:&sharpinclude ''stm8s.h''&sharpdefine I2C_SPEED 300000&sharpdefine OWN_ADDRESS 0xA0 &sharpdefine SLAVE_ADDRESS 0x30void delay_delay(unsigned int mul);void main(){ CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1); I2C_DeInit(); I2C_Init(I2C_SPEED, 0xA0, I2C_DUTYCYCLE_2, I2C_ACK_CURR, I2C_ADDMODE_7BIT, 16);while (1){ I2C_GenerateSTART(ENABLE);I2C_Send7bitAddress(SLAVE_ADDRESS, I2C_DIRECTION_TX);I2C_SendData(0x61);I2C_GenerateSTOP(ENABLE);delay_delay(500);}}void delay_delay(unsigned int mul){ for(; mul>0; mul--);}&sharpifdef USE_FULL_ASSERTvoid assert_failed(uint8_t* file, uint32_t line){ while (1) {}}&sharpendif/*******************************************************************/Slave:&sharpinclude ''stm8s.h''&sharpinclude ''stm8s_uart3.h''&sharpinclude ''stdio.h''&sharpinclude ''stm8s_i2c.h''&sharpdefine I2C_SPEED 300000&sharpdefine OWN_ADDRESS 0xA0 &sharpdefine SLAVE_ADDRESS 0x30void delay_delay(unsigned int mul);void sendstring(char *s){ while(*s){ UART3->DR = (u8) (*s); while ((UART3->SR & (u8) UART3_FLAG_TXE) == RESET); s++; } }void main(void){CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);UART3_DeInit();UART3_Init((uint32_t)9600, UART3_WORDLENGTH_8D, UART3_STOPBITS_1, UART3_PARITY_NO, UART3_MODE_TXRX_ENABLE);I2C_DeInit();I2C_Init(300000, 0x30, I2C_DUTYCYCLE_2, I2C_ACK_CURR, I2C_ADDMODE_7BIT, 16);char veri_bas[1]; while (1){ I2C_AcknowledgeConfig(DISABLE);uint8_t data = I2C_ReceiveData(); //-datayy okuI2C_AcknowledgeConfig(ENABLE);sprintf(veri_bas ,''%i'' ,data);sendstring(veri_bas);delay_delay(500);}}void delay_delay(unsigned int mul){ for(; mul>0; mul--);}&sharpifdef USE_FULL_ASSERTvoid assert_failed(uint8_t* file, uint32_t line){ while (1) {}}&sharpendifIt does not work. Help please, I can't find the error.Also:Resistors(4.7K) are okey for I2C Communication. #stm8s208 #hal #stm8s-i2c #i2c