STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S, how to active multiTouchs at the same time?

Posted on June 13, 2016 at 09:18Dear All,I use  <<STM8S_TouchSensing_Lib_V2.5.0_setup.exe>> to build one testing system of STM8S RC Touchsensing. it has four ''buttons'' and four LEDs. for every ''button'', it can works well for touching. once the h...

newbie question about Morpho connector

Posted on June 29, 2016 at 04:57Hi All   I am new to stm32 nucleo board, the pins on morpho connector are I/O pin? Or they are used to connect to expansion board only?thanksfrom Peter

TIM1 PWM Input

Posted on May 02, 2013 at 11:25Dear All, I am trying to measure the frequency (and duty cycle) of a 1 kHz to 2 kHz signal which is connected to PD4 using TIM1 capture capability. As far as I can see from the documentation PD4 is connected to TIM1.IC...

wynand by Associate II
  • 1570 Views
  • 6 replies
  • 0 kudos

A list of RTOSes relevant to the STM8 and their availability

Posted on June 23, 2016 at 21:29I just compiled a quick availability list of RTOSes that are relevant to the STM8 (by having an STM8 or ST7 port, or just being one of the most important RTOSes out there). The list features availability aspects: Lice...

ST-Link V2 STM8S Program Problem

Posted on June 20, 2016 at 13:23Hai,    I have write code for LED blinking for STM8S105K4. I try to program it through ST-Link V2 adapter. But it shows warning as 'Warning : FILE : line 1: Address 0x4800 is out of range and is ignored!'.       I hav...

STM8 Bootloader enabling

Posted on June 19, 2016 at 14:54Hi all,I want to enable the STM8AF5289 bootloader for downloading the application through serial port. I have downloaded the ST visual programmer for this purpose .Can anyone please provide me the steps to be done for...

CAN received message filtering mechanism

Posted on June 10, 2016 at 14:03Hi all,I am working on some CAN communication project which allows us to control some external device attached to one node from some other node.Since the CAn bus is a broadcast network and hence a message sent by a no...

amitkrv22 by Associate II
  • 1259 Views
  • 1 replies
  • 0 kudos

STM8L151F3 high failure rate

Posted on June 16, 2016 at 16:34Situation: Chip STM8L151F3U6.Circuit = MCU + LED (work time counter) After manual assembly, we have 80% of the output of defective products.Current consumption in reset from 0.1 mA to 8 mA (from sample to sample).Powe...

0690X00000602o3QAA.jpg

Small Device C Compiler 3.6.0 released

Posted on June 13, 2016 at 00:54Version 3.6.0 of SDCC, a C implementation targeting 8-bit architectures including the STM8 was released a few hours ago: Today a new release of SDCC was made. We are now at version 3.6.0. You can get it at: http://sou...

STM8L152R8 LCD Controller

Posted on June 12, 2016 at 05:43Hello,I'm currently working on STM8L152R8 and I need to drive a customized LCD glass. The problem is that I can not find any information about LCD_RAM[22:0] bits versus associated segments. For example I don't know wh...