2016-06-11 08:43 PM
Hello,
I'm currently working on STM8L152R8 and I need to drive a customized LCD glass. The problem is that I can not find any information about LCD_RAM[22:0] bits versus associated segments. For example I don't know which LCD_RAM[x] bit is related to segment 1, COM 1. Is there application note about this? By the way I've read the AN3114 application note (which is about driving LCDs on evaluation boards) and there is nothing about this.Thanks in advance