cancel
Showing results for 
Search instead for 
Did you mean: 

Small Device C Compiler 3.6.0 released

Philipp Krause
Senior III
Posted on June 13, 2016 at 00:54

Version 3.6.0 of SDCC, a C implementation targeting 8-bit architectures including the STM8 was released a few hours ago:

 

Today a new release of SDCC was made. We are now at version 3.6.0. You can get it at:

http://sourceforge.net/projects/sdcc/files/

So what's new? * Merged upstream binutils 2.25 * New memory management with lower overhead * Changed default language dialect to --std-sdcc11 * Diagnostic for missing type specifier: No implicit int outside of C90 mode anymore * C11 generic selections * char type is now unsigned by default (old behaviour can be restored using --fsigned-char) * Character constants are now of type int instead of char. * ISO C95 and ISO C11 wide character constants * ISO C95 and ISO C11 wide string literals * Basic standard library support for wide characters: c16rtomb(), mbrtoc16(), mbsinit(), mbtowc(), mbrlen(), mbrtoc32, c32rtomb(), mbrtowc(), wcrtomb(), mblen(), wctomb() * Treat all ports the same in the manual (i.e. mcs51-specific stuff is now clearly described as such) * Reorganized interrupt handling for z80, z180, r2k, r3ka, tlcs90, gbz80 backends * Workaround for stm8 division hardware bug * ELF/DWARF support for stm8 * Output symbol table for ELF * pic16 port now uses standard-compliant crt0iz that initializes static and globals to 0 by default And of course numerous feature requests and bug fixes are included as well. Once again I hope you will enjoy using this new release. Maarten Brock SDCC 3.6.0 Release Manager

 

 

Most important to STM8 users are probably the improved standard support and various small fixes and improvements in the STM8 backend.

A current comparison of C compilers for the STM8 can be found at

http://colecovision.eu/stm8/compilers.shtml

.

Philipp
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Philipp Krause
Senior III
Posted on June 15, 2016 at 10:11

At FOSDEM 2015, there was a talk on SDCC:

https://archive.fosdem.org/2015/schedule/event/8bit_compiler/

There is also a blog post on what happened in SDCC since the talk up to the SDCC 3.6.0 release:

http://www.embecosm.com/2016/06/14/recent-updates-to-sdcc-in-release-3-6-0/

Philipp