cancel
Showing results for 
Search instead for 
Did you mean: 

STM8L101 clocking at < 2 MHz

Dmitry A
Associate
Posted on October 15, 2015 at 15:12

Hello All, 

Is there any way to run STM8L101 at a frequency about 200 kHz to save some microAmps?

BR, Dmitry

#frequency #stm8l101
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Ian Legg
Senior
Posted on October 19, 2015 at 10:04

Hi Dimitry,

The L101 only looks to have the internal 16MHz RC clock, so an external crystal is not possible. However, you could adjust the CLK_CKDIVR to 64 for a 250KHz clock.

Hope that helps.

Ian

toppot2009
Associate II
Posted on October 25, 2015 at 13:15

Добрый день, Дмитрий

В stm8l101 �?огла�?но референ�? мануал не уда�?т�?�? уменьшить тактовую ча�?тоту ниже 2 МГц при и�?пользовании HSI (внутреннего RC генератора). Един�?твенна�? возможно�?ть уменьшени�? потреблени�? до микроампер �?то и�?пользовать режим Active-halt �?овме�?тно �? Auto-wakeup.