Posted on August 03, 2017 at 09:40Hello,It's my understanding that the LSI clock is always on because it's used for the SWIM functionality? If it isn't then naturally it needs switching on and routing to the RTC with the appropriate dividers set. I'...
Posted on June 12, 2017 at 09:36Hi David,I think this is related to either the version of STVD you have or whether you install STVD or the STLink v2 driver first. I'm sure there is a posting about it somewhere Thanks,Ian
Posted on March 23, 2017 at 10:19Hello,Presuming you are using an ST-link v2, have you got it connected correctly, are the drivers installed, is STVD configured to use it etc?The second error is because CLK_SWR (and the others) are not defined. The ...
Posted on March 01, 2017 at 09:19Hello,I would suggest that a while loop delay in an isr is not good practice but I also note that you aren't re-initializing the 'i' variable so you'll get strange effects there.It might be better to use PWM, that wa...
Posted on December 16, 2016 at 10:05Hi Seb,Sorry this is the first time I've used the new forum setup. My reply was intended for Jeremy, I hadn't looked at your example.Thanks,Ian