STM8L Timer Initiation problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-12 5:21 PM
Hello,
I am new to ST processors. Here is the issue:
I am trying to setup Timer 3 for interrupt, Code:
TIM3_DeInit();
CLK_PeripheralClockConfig(CLK_PCKENR1_TIM3, ENABLE);
TIM3_TimeBaseInit(TIM3_Prescaler_64, TIM3_CounterMode_Down, 2500);
TIM3_SetCounter(0);
TIM3_ARRPreloadConfig(ENABLE);
TIM3_PrescalerConfig(TIM3_Prescaler_64,TIM3_PSCReloadMode_Update);
TIM3_ITConfig(TIM3_IT_Update,ENABLE);
TIM3_Cmd(ENABLE);
The funny thing is that the call "CLK_PeripheralClockConfig(CLK_PCKENR1_TIM3, ENABLE);" does not turn the Timer 3 gate on. As a matter of fact it turns on gate for Timer 4.
I had to use "CLK_PCKENR1_TIM2" to turn on the gate for Timer 3.
I traced to the function and fund this line inside "CLK_PeripheralClockConfig" (stm8l15x_clk.c)
" CLK->PCKENR1 |= (uint8_t)((uint8_t)1 << ((uint8_t)CLK_Peripheral & (uint8_t)0x0F)); "
The shift "1 <<" operation will always enable the gate for the device next in line!
That is why I have to use CLK_PCKENR1_TIM2 to turn on the gate for Timer 3. Based on this there is no way to make TImer 2 work by calling this function.
Am I right?
Thanks.
Tony
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-14 6:13 PM
Please ignore my last post.
I found the problem is that when "CLK_PeripheralClockConfig(CLK_PCKENR1_TIM3, ENABLE);" is called the "CLK_PCKENR1_TIM3" gets changed to "CLK_PCKENR1_TIM4" inside the function.
It is very strange and did "rebuild all" and problem still persists. I checked another instance of this function and no problem there.
I'll see if rewrite/retype the section helps.
Tony