STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

raisonance rlink stm8 stvp cannot communicate with the tool

Hello, I am trying to program a stm8l151c8 with Raisonance but I get the following message: Cannot communicate with the tool. Wrong tool selection or check tool power supply or check that a previous session is closed. Do I need to change any jumper o...

VYoun by Associate III
  • 1359 Views
  • 1 replies
  • 0 kudos

In order to make some gang programmer for the STM8 parts we want to use a STM32 processor. Is there public code available which does implements the SWIM interface on the STM32 parts ?

In order to create a gang programmer we were thinking of using multipe STM32 processors were every processor implements the SWIM interface in order to program STM8 processors in parallel. We can we find code written for a STM32 device which implement...

STM8S001J3M3 pull-up resistor value on PB4

In an application we use PB4 as output. Corresponding to the datasheet, this port only can be used with open-drain. In the datasheet in the I/O port pin characteristics there are values of 30k up to 80k for pull-up resistor Rpu. Is this meant for the...

AZehn.1 by Associate
  • 1010 Views
  • 1 replies
  • 0 kudos

code development manual for STM8L

Hello,I am using NUCLEO-8L152R8 board for our project purpose.I am new to this board. I have downloaded tools like STM8Cubemx, ST visual develop.I haven't found any video or document which will guide me on how to develop code in ST visual develop and...

DJosh.0 by Associate II
  • 903 Views
  • 2 replies
  • 0 kudos

8-pin part label part identification (ST G9949)

I'm trying to identify an 8-pin part that appears to have an "ST" logo on it. I'm pretty sure it is an 8-bit MCU, (part of a LED tube driver dimmer control) The part numbers looks like ST G9949, but I can't find a match on ST.com. Does ST custom labe...

0693W000007CQk7QAG.png
DMatt.2 by Associate II
  • 1156 Views
  • 1 replies
  • 0 kudos

STVD user manual

Hey, The STVD latest version available from the Website is 4.3.12. But its user manual On the Website (Doc: UM0036) is for STVD version 4.0.1 (Which is released in 2010).I can't find any User Manual DOC for STVD latest Version 4.3.12.anybody any Idea...

KGupt.1 by Associate III
  • 701 Views
  • 2 replies
  • 0 kudos

Hi, I´m using STM8S0003F. I have 2 pins at PORT A (PA1 and PA3 that are programmed to generate an interrupt when any signal FALL_ONLY. During the interrupt routine, how can I know which pin generate this interrupt? Thank you Andre

INTERRUPT_HANDLER(EXTI_PORTA_IRQHandler, 3){ /* In order to detect unexpected events during development,   it is recommended to set a breakpoint on the following instruction. */ if(!GPIO_ReadInputPin(RUIDO_PASS_Port, RUIDO_PASS_Pin)) { Tmr10msLeRuid...

AMast by Associate
  • 495 Views
  • 0 replies
  • 0 kudos