2020-09-07 10:51 AM
My following code is not working for sending data over LINUART port of STM8AF5286. I am using STVD and STM8_Standard_Project_Template.
GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_OUT_PP_HIGH_FAST);
UART3_DeInit();
UART3_Init(9600,UART3_WORDLENGTH_8D,UART3_STOPBITS_1,UART3_PARITY_NO,UART3_MODE_TX_ENABLE);
UART3_Cmd(ENABLE);
UART3_SendData8(0xAA);
Can you please guide me as why data (0xAA) is not coming out on PD5 pin of microcontroller?
2020-09-07 12:12 PM
Make sure GPIOD and UART3 clocks are enabled prior to configuration
2020-09-08 1:35 AM
Yes...clocks are enabled for all peripherals.
CLK->PCKENR1 = 0xFF;
CLK->PCKENR2 = 0xFF;
I tested GPIO Port D pin5 to go high and low as i write high or low through the code .
One more input - As i am using STM8AF5286 and in STM8 standard library i do not see any #define for STM8AF528x controllers and hence i have uncommented STM8AF52Ax in stm8s.h file. Please refer below section from this file.
/* Uncomment the line below according to the target STM8S or STM8A device used in your
application. */
/* #define STM8S208 */ /*!< STM8S High density devices with CAN */
/* #define STM8S207 */ /*!< STM8S High density devices without CAN */
/* #define STM8S007 */ /*!< STM8S Value Line High density devices */
#define STM8AF52Ax /*!< STM8A High density devices with CAN */
/* #define STM8AF62Ax */ /*!< STM8A High density devices without CAN */
/* #define STM8S105 */ /*!< STM8S Medium density devices */
/* #define STM8S005 */ /*!< STM8S Value Line Medium density devices */
/* #define STM8AF626x */ /*!< STM8A Medium density devices */
/* #define STM8AF622x */ /*!< STM8A Low density devices */
/* #define STM8S103 */ /*!< STM8S Low density devices */
/* #define STM8S003 */ /*!< STM8S Value Line Low density devices */
/* #define STM8S903 */ /*!< STM8S Low density devices */
/* #define STM8S001 */ /*!< STM8S Value Line Low denisty devices */