2016-07-01 04:17 AM
my fCPU is16MHz.
In order to get 500K baudrate, I have programmed as follows: CAN_SynJumpWidth = CAN_SynJumpWidth_1TimeQuantum; CAN_BitSeg1 = CAN_BitSeg1_8TimeQuantum ; CAN_BitSeg2 = CAN_BitSeg2_7TimeQuantum; CAN_Prescaler = 2; On the other end, I use CANOE to view the transmitted messages, which is also configured to the same baud rate. But when I check the transmission status, the messages are still in the mailbox. It works in the loopback mode. What could I be missing? Thanks #bxcan #stm8/128