2013-04-10 07:13 AM
STLED316S
I would like some clear instructionsthat inform me how to communicate with the STLED316S.
I have the STEVAL-ICB003V board,viewing the communications on a logic analyzer, and attempting to duplicate the setup does not work.
I am connected to the STLED316S with a uC, can get only DIG1_LED to illuminate.
Is there is someone at ST that knows how to point to a memory location and write control values, please do share?
An example that tells how to set the STB line low while pointing to a memory location + page file would be useful.
Example, write to STLED316S to set number of digits, then set to send series of values to each digit for display.
In addition, I am using 3.3V for the serial communications, I am powering the STLED316S with 5V, and pulling DIN/DOUT up with 3.3V. Is this the proper method?
2013-04-10 12:42 PM
Please see STM32 forum for the conclusion to these struggles with documentation.