STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EWSTM8 of IAR - problems with debugging

Posted on September 21, 2012 at 10:33Dear,In the past I published here in the forum a question about EWSTM8 problems.I have been in touch with IAR on that and now I have their Beta version. This beta version has solved a problem with crashes as resu...

elil by Associate III
  • 3382 Views
  • 0 replies
  • 0 kudos

Software Update on STM8

Posted on September 12, 2012 at 12:40I am working on a low density STM8S with 8Kbyte flash memory. I need to accomodate a main software and a recovery software. I do not need any special bootloader as I am planning to make the software update as pa...

spveer by Associate II
  • 1205 Views
  • 3 replies
  • 0 kudos

ICP and IAP: Linker

Posted on September 18, 2012 at 17:21 Hi, Is it possible to program only part of the flash memory using ICP? I have STM8 programmed with bootloader using ICP where UBC is protected from 0x8000 to 0x8fff. Now when I try to...

spveer by Associate II
  • 541 Views
  • 0 replies
  • 0 kudos

TIM3 wrong counting?

Posted on September 04, 2012 at 17:14I need to generate a 20 ms interrupt into my firmware. HSE is 16 Mhz with STM8S208. I put this initialization code into my firmware to accomplish that through the use of TIM3: #define PRESC TIM3_PRESCALER_32     ...

STVD 4.3.1 : swim error [30103]

Posted on February 09, 2012 at 12:26Hi, I'm running windows 7 64 bit, my target is STM8S103F2U. STVD gives me this error when trying to debug: ''failed to download application: error: swim error [30103]: rlink communication error''.    Rlink does no...

@eeprom

Posted on August 09, 2011 at 18:31Anyone know how to use the @eeprom on the cosmic compiler Does it suppot @eeprom vu32 EE_Total; The above passed the complier but if I try to use it I get errors I've also tried char and int but none seem to work. ...

Debug/programming another chip with STLINK from STM8disco

Posted on August 30, 2012 at 12:11Hi, After developping and testing with stm8s-discovery connected to various evalboards, i just received my prototype. As written in STM8SVLDISCOVERY's usermanual, i unsoldered the two 0 Ohms of swim connector from t...

thibaut2 by Associate II
  • 684 Views
  • 1 replies
  • 0 kudos

Breadboard friendly to the STM8L-Discovery?

Posted on August 20, 2012 at 10:30I've got an STM8L-Discovery and am having loads of fun with it.  I would like to go beyond flashing two LEDs and writing stuff to the LCD display, however, which means I'd like to breadboard.  The problem is that th...

STM8S003F3 chip and GPIO

Posted on August 15, 2012 at 04:33Hi all! I'm working with STM8S003F3 chip on my project and I'm have some problem about it, i wana help of ST technician. on my project,i using pin4 and pin5 of port B to control normal IO applications,I have alrea...

ST Visual Develop Multiple Instance Issue

Posted on July 26, 2012 at 09:57Hi Guys,I'd like to work on multiple projects at the same time using STVD. But it does not permit to open a second instance. I dug in to the options and help, but couldn't find any clue about this subject. Is there a ...