cancel
Showing results for 
Search instead for 
Did you mean: 

st link v2 stm8 not reset

David.Cheng
Associate II

after program the mcu by STVP, the mcu does not reset and start up, why?

swim does not have reset function?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John7
Associate II

Hi David,

I have the ST-LINK V2/ISOL.

At least these 2 conditions must be met:

1. You also need to connect the ST-LINK-V2 RESET pin to the target MCU RESET pin !

Make sure to have all connections in user manual UM1075, par. 3.1.3 "SWIM signals and connections", table 2.

2. The ST-LINK-V2 RESET pin must be ABLE to pull the MCU-RESET pin low enough.

So if you drive the target MCU-RESET pin by a push-pull driver or your pull-up resistor is very low,

the ST-LINK-V2 RESET pin driver might not reach a sufficent low level to cause a MCU reset.

The ST-LINK-V2 RESET pin is an input and an open drain output with a 680 Ohm pull-up.

Best use a wired-or aproach on your target board.

Hope this helps,

John