How can i get the schemetic of MB1440B by STLINT V3 set ?
Hi: Mostly the Stlink V3 set seems like a develop board , i am realy need more information about the MB1440B , So how can i get the schemetic ? thanks a lot .
Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.
Hi: Mostly the Stlink V3 set seems like a develop board , i am realy need more information about the MB1440B , So how can i get the schemetic ? thanks a lot .
INTERRUPT_HANDLER(USART1_TX_TIM5_UPD_OVF_TRG_BRK_IRQHandler,27) { /* In order to detect unexpected events during development, it is recommended to set a breakpoint on the following instruction. */ USART_SendData8(USART1, TxBuffer[T...
when i am using 8 bit microcontrollers, i use compilers that have a lot of libraries to make my work in programming the micrcontroller very easy, e.g lcd library and a lot of libraries so the development of my code will be easy, in fact i am trying t...
Hello! I'm learning to code an STMicroelectronics 8 bit micro-controller. I want to control a BLDC motor with this MCU for electric vehicle application. I'm using the STM8S DISCOVERY Board, based on the STM8S105C6T6 (48 pin) MCU. This MCU has 4 timer...
Hi.I have faced a weird problem using IAR compilers.Errorstatus=0; Relay_Off; delay_ms(200); if(Errorstatus==1){ Errorflag=1;In this part of my code after I switch the relay off, I put a delay and if an interrupt...
I have Nucleo-L152RE board and I used this board to program the STM32 MCU using JTAG (CN4) connector. Now, I want to program the STM8 board using SWIM interface. So, is it possible with Nucleo-L152RE?. I already done the required changes to use Nucle...
float get_resi(void) in https://gist.github.com/goog/bf784c5f63a199ddbde7cd49db92f73fcould you help to check the get_resi function?im not sure whether my time counter has some issue?
I am working on my first STM8 project and getting used to its own flavour of quirks etc.Setting up a new project installs stm8s_interrupt_vector.c which I understand. I want to use the standard peripheral drivers so have downloaded them and added the...
static void TIM1_Config(void) { CLK_PeripheralClockConfig(CLK_Peripheral_TIM1, ENABLE); TIM1_DeInit(); // 2m/ 40 TIM1_TimeBaseInit(39, TIM1_CounterMode_Down, 0xffff, 0); //timer freq = (clock CPU/16) -> 1bit = 1uS -> 92...