2016-07-25 03:39 AM
Code speed results didn't look that good for SDCC at the time of the SDCC 3.6.0 release about a month ago (http://colecovision.eu/stm8/compilers.shtml). But SDCC has made huge progress since, and now achieves higher Dhrystone and Coremark scores than the other compilers. Here are the results for the current development version (SDCC 3.6.2 #9667):
2016-12-07 04:30 AM
Very interested. Version 3.6.2 will be accessible for free?
2016-12-08 05:18 AM
SDCC is free. The previous release is 3.6.0, the next release will be 3.7.0 (probably in the first half of 2017). 3.6.2 is a developmental version, not a release version, so you'd have to build it yourself. The most recent snapshots of developmental versions are available at
http://sdcc.sourceforge.net/snap.php
as source, Windows and Linux binaries, but they haven't undergone as much testing as the releases.Philipp
2016-12-08 06:08 AM
Ok. Thanks for explanation.
2016-12-11 11:25 PM
Hello, Philipp.
Excuse me persistence. Now I try make workable test by SDCC. But have some
unresolved issues. The lack of optimization require to write rules for peephole. But I would like to have developed and ready to use definitions. It can be accessible? It is not clear, how to determine the vector interrupt of trap. If you can, tell please.
Sincerely, Viacheslav.2016-12-12 04:48 AM
The trap handler is declared using the __trap keyword where normal user interrupts use __interrupt(N):
void handler(void) __trap
{ … }As for normal interrupts, a declaration for the handler needs to be in the same file as main().
This information is missing from the SDCC 3.6.0 manual. In the current development version it is in section 3.6.7 ('STM8 Interrupt Service Routines'), and will thus be in the SDCC 3.7.0 manual.
Philipp
2016-12-12 04:55 AM
Viacheslav Azarov schrieb:
The lack of optimization require to write rules for peephole. But I would like to have developed and ready to use definitions. It can be accessible? […]
I'm not sure what you mean here. SDCC has peephole rules that are used for optimization (unless you specify --no-peep). While it is possible to specify additional peephole optimizer rules using --peep-file that should not be necessary for typical use.
The most important options for optimization for STM8 are:
* --opt-code-size to optimize for code size (possibly resulting in slower code)
* --opt-code-speed to optimize for code speed (possibly resulting in bigger code)
* --max-allocs-per-node N (higher values for N result in better code, but slower compilation; the default for N is 3000)
Philipp
2016-12-12 06:17 AM
Thank You for reply.
I tried all optimisation options for 3.6.0 version, but this has no effect.
Until I not applied the peephole file that was written relative to outcome.
And about __trap, thanks. But it would be better to save indexes of native
vector table.
...
Application of the native peephole file does not give expected result.
Code still contains unnecessary instructions. Attachment contains one example.
Hopefully that in version 3.7.0 everything will be beautiful.
Sincerely, Viacheslav.
2016-12-12 13:56 GMT+02:00 krause.philipp <
mailto:st-microelectronics@jiveon.com
>:
STMicroelectronics Community
<
https://community.st.com/?et=watches.email.thread
>
Re: SDCC generates the fastest integer code for STM8
reply from krause.philipp
<
https://community.st.com/people/Krause.Philipp?et=watches.email.thread
>
in STM8 MCUs - View the full discussion
<
https://community.st.com/thread/8847?commentID=139256&et=watches.email.thread#comment-139256
>
________________ Attachments : stm8opt.txt.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hz2m&d=%2Fa%2F0X0000000bFm%2FhLJtWxn.VM1gRR54iWANO4RGS0_KZ627DOCEryeW6.s&asPdf=falsepeephole.def.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyqd&d=%2Fa%2F0X0000000bFj%2FY8xo2m9Ry4DTXbGEMeAUbyaWYCZi3B4x403N2qwtFoA&asPdf=falselacksdcc.txt.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hz2h&d=%2Fa%2F0X0000000bFk%2FkBI4LZ61Iuq9ZtFOrsTnuFO5i8gArY9fNvmQWkNxHP4&asPdf=false2016-12-17 02:07 PM
Application of the native peephole file does not give expected result.
Code still contains unnecessary instructions. Attachment contains one example.
Unfortunately it is not that simple. Your stm8opt.txt contains 4 rules for the peephole optimizer.
The first and second could incorrectly remove accesses to volatile variables. If the check for volatile is added, they become equivalent to existing official rules 1 and 1w.
The third rule is correct, but I haven't yet found code to which it would apply in the SDCC output.
The fourth rule does not preserve flags N and Z.
Philipp
2016-12-18 08:35 AM
Hello, Philipp.
I understand problems of optimisation algorithms. It is really complex. I
am not specialist in this field. And my four rules has been written for
experiment only. But native rules that from source have same effect.
Viacheslav.
2016-12-17 23:07 GMT+02:00 krause.philipp <st-microelectronics@jiveon.com>:
STMicroelectronics Community
<https://community.st.com/?et=watches.email.thread>
Re: SDCC generates the fastest integer code for STM8
reply from krause.philipp
<
in STM8 MCUs - View the full discussion
<https://community.st.com/0D70X000006T1B6SAK