2020-12-25 10:52 PM
Hi,
Reset is not happening at only particular project while debugging using STVD. But the same code is working fine if I load the code through STVP. Same MCU Reset is working fine with other project while debugging. I don't know is there any settings need to be changed in the STVD. I commented all the lines except CLOCK INTZ but still in that project, reset is not happening. If I manually short the RESET and GND pins means Reset is happening but through STVD not happening. Help me to solve this problem...
MCU: STM8S003K3
Regards,
Nishanth M