2019-10-02 11:09 PM
I'm trying to use TIM1 to output a PWM signal on stm8s103f3 using the standard library (patched) with sdcc compiler.
The output goes high, but there's no signal.
#include "stm8s.h"
#include "stm8s_it.h" /* SDCC patch: required by SDCC for interrupts */
signed int PWM_DUTY = 500;
void main (void) {
clock_setup();
TIM1_Setup();
GPIO_Setup();
while(1) {
TIM1_SetCompare1(PWM_DUTY);
}
}
void GPIO_Setup(void) {
GPIO_DeInit(GPIOC);
GPIO_Init(GPIOC, GPIO_PIN_3 | GPIO_PIN_6, GPIO_MODE_OUT_PP_HIGH_FAST); //enable output on PC3
}
void clock_setup(void) {
CLK_DeInit();
CLK_LSICmd(DISABLE);
CLK_HSECmd(DISABLE);
CLK_HSICmd(ENABLE);
CLK_ClockSwitchCmd(ENABLE);
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1); //8MHz clock
CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSI, DISABLE, CLK_CURRENTCLOCKSTATE_ENABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1, ENABLE);
}
void TIM1_Setup(void) {
TIM1_DeInit();
TIM1_TimeBaseInit(16, TIM1_COUNTERMODE_UP, 1000, 1);
TIM1_OC1Init(TIM1_OCMODE_PWM1, TIM1_OUTPUTSTATE_ENABLE, TIM1_OUTPUTNSTATE_ENABLE, 1000, TIM1_OCPOLARITY_LOW, TIM1_OCNPOLARITY_LOW, TIM1_OCIDLESTATE_RESET, TIM1_OCNIDLESTATE_RESET);
TIM1_CtrlPWMOutputs(ENABLE);
TIM1_Cmd(ENABLE);
}
Am I missing something or is it the library?
2019-10-03 12:39 AM
Hello,
You have configured the same value for period and pulse, thus you cannot see PWM on the pin.
Please replace 4th argument (1000) within TIM1_OC1Init() with PWM_DUTY and it should work.
Best Regards,
Artur
2019-10-30 8:50 AM
Also, take into account pin 16 (aka PC6) only operates as TIM1_CH1 when option bit OPT2.AFR0 is set and NOPT2.NAFR0 is cleared. Otherwise, you will get no signal since that pin would be operating as SPI_MOSI instead.
2019-11-11 11:45 AM
Thanks! Your remark about the option-bits did help me, as I was wondering why TIM1 CH1 didn't produce any output.
(But that pin would be MOSI only if SPI was enabled, right?)
Wilko
2019-11-11 12:26 PM
Exactly. According to the STM8S003K3/F3 datasheet, the default function after reset for that pin is PC6, so it acts as a simple GPIO pin.
2019-11-12 3:58 AM
Yes, it is in the Datasheet, but why isn't it in the Reference guide ST?
Wilko