cancel
Showing results for 
Search instead for 
Did you mean: 

Program STM8 flash

New.Fish
Associate III

Can I use "STM32 ST-Link Utility" or "STM32CubeProgrammer" to program STM8MCU flash?

If using "STVP", can it automatically detect the STM8MCU type? or require to configure "STVP" for the MCU type to be programmed.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

As can be seen from the name, STM32 ST-Link Utility and STM32CubeProgrammer can only be used for STM32.

STVP cannot automatically determine the target MCU, so it must always be specified.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

As can be seen from the name, STM32 ST-Link Utility and STM32CubeProgrammer can only be used for STM32.

STVP cannot automatically determine the target MCU, so it must always be specified.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.