2019-09-25 1:54 PM
2019-09-25 3:03 PM
Not sure you've got something that does both well. Keil can build other code (ie start compilers, linker) via user command options from a primary project.
Probably other source management / static analysis tools or editors that could do an effective job. Perhaps Visual Studio would allow multi-target projects, or at least form a common editor function.
IAR looks to support both, not sure the level of integration across multiple targets.
2019-10-06 2:37 AM
I can see the advantage of not having to learn to different IDEs, and of implementation-defined behaviour being similar for both compilers.
So Keil is out. AFAIK, Cosmic supports ARM. AFAIK, Raisonance also supports both ARM and STM8, but these days (and already since a few years), Raisonance is not considered a good choice for STM8 unless you value code size above everything else (see e.g. the comparison of STM8 C compilers at http://www.colecovision.eu/stm8/compilers.shtml).
Since IAR supports both, it could be an option.
I would use free tools for both, i.e. SDCC for STM8, GCC or LLVM for STM32. There are free IDEs, that support all those compilers, e.g. Code::Blocks.