2024-01-21 5:00 AM - edited 2024-01-21 10:41 AM
Hello stm community. I am designing my first ever PCB board and i need some comments of yours. Here is the screenshots of the pcb schematic and pcb itself. Do you see any mistakes etc? Also I am not sure about the VCAP connection. Is it correctly made?
2024-02-06 3:16 AM
Actualy i am planning to fill the vias with solder so that it can conduct better. I have seen people doing this? Is this a bad practice?
2024-02-06 5:04 PM
It is not good practice. If this was a board to be assembled by a CM (contract manufacturer) it would have solder paste applied by a stencil. The stencil has a thickness depending on the components on your board. Not a lot of paste goes onto the pads with a stencil (with a TQFP footprint) so the solder will go down the hole(s) and not the pin you're trying to solder. You have plenty of space to avoid the vias in pads.
2024-02-07 12:47 AM
You are right. If this was to be assembled by the manufacturer this would not be suitable. Thank you.