Is there any pre-requirments on using PC0 & PC1 as GPIO PP in STM8L051?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-09 6:22 PM
Hi all,
I am trying to use STM8L051 port c pin 0 as an output to drive a NPN. But I find that PC0 & PC1 cannot be set by using ST HAL library. All the registers seems ok (DDR, ODR, CR1 & CR2). And PC4,5,6 can be driven. Can anyone please give me a hand by providing some hints? AHere are the code:
#include "stm8l15x.h"
#include "main.h"
void delay_ms(uint16_t u16_ms)
{
for(uint16_t u16_a = 0; u16_a < u16_ms; u16_a++)
{
for(unsigned short u8_a = 0; u8_a < 37; u8_a++)
{
nop();
}
}
}
void main(void)
{
CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_64);
/* Select HSI as system clock source */
CLK_SYSCLKSourceSwitchCmd(ENABLE);
CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSI); // CLK_SYSCLKSource_HSI
while (CLK_GetSYSCLKSource() != CLK_SYSCLKSource_HSI);
GPIO_Init(GPIOC,GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6, GPIO_Mode_Out_PP_Low_Slow);
while(1)
{
GPIO_SetBits(GPIOC,GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6);
delay_ms(1000);
GPIO_ResetBits(GPIOC,GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6);
delay_ms(1000);
}
}
Solved! Go to Solution.
- Labels:
-
GPIO-EXTI
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-11 12:51 AM
Oops, sorry, I got it mixed up with the STM8S family library.
You are right, of course, but you should take into account that on the STM8L051 exactly two pins are so-called true open drain ports - PC0 and PC1. The RM0031 writes about this:
In the true open-drain I/Os, P-Buffer, weak pull-up and protection diode to VDD is not implemented.
This means: to drive an H-level at the output, you must connect an external pull-up, which provides the driving current for your npn BRT.
Regards
/Peter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-10 1:22 AM
Welcome, @SSin.1​, to the community!
For NPN you need an open-drain output. If you initialise the pins in line 25 as PP (push-pull), however, you logically have a push-pull output and no open-drain.
For initialisation instead of
GPIO_Mode_Out_PP_Low_Slow
please use e.g.
GPIO_Mode_Out_OD_HiZ_Slow
Hope that helps?
Regards
/Peter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-10 1:30 AM
Thanks for your help.
Sorry for my poor explaination, what I mean is something tlike this:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-10 2:10 AM
Oh, I thought by NPN you meant an NPN of a PLC.
Please try it and replace
GPIO_SetBits(GPIO_TypeDef* GPIOx, uint8_t GPIO_Pin)
by
GPIO_WriteHigh(GPIO_TypeDef* GPIOx, GPIO_Pin_TypeDef PortPins)
...and accordingly for GPIO_ResetBits --> GPIO_WriteLow.
Please note that GPIO_SetBits and GPIO_ResetBits with uint8_t requires a different type for the GPIO_Pin than GPIO_WriteHigh and GPIO_WriteLow (GPIO_Pin_TypeDef).
Regards
/Peter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-11 12:35 AM
Dear Peter,
Thanks a lot! But can you please kindly tell me where can I get the lastest ST offical HAL w/ GPIO_WriteHigh function? The version on my hand is v1.6.1, which doesn't contain GPIO_WriteHigh.
* @file stm8l15x_gpio.c
* @author MCD Application Team
* @version V1.6.1
* @date 30-September-2014
BTW, GPIO_SetBits has just one line
void GPIO_SetBits(GPIO_TypeDef* GPIOx, uint8_t GPIO_Pin)
{
GPIOx->ODR |= GPIO_Pin;
}
And it can change ODR. So what can I do to modity the function to make it works? Thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-11 12:51 AM
Oops, sorry, I got it mixed up with the STM8S family library.
You are right, of course, but you should take into account that on the STM8L051 exactly two pins are so-called true open drain ports - PC0 and PC1. The RM0031 writes about this:
In the true open-drain I/Os, P-Buffer, weak pull-up and protection diode to VDD is not implemented.
This means: to drive an H-level at the output, you must connect an external pull-up, which provides the driving current for your npn BRT.
Regards
/Peter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-11 12:53 AM
Dear Peter,
Thanks a lot! sorry for missing such a point!