Install STM8CubeMX Issues
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-03-30 7:28 PM - edited 2024-03-30 7:40 PM
Getting stuck installing STM8CubeMX on Ubuntu 23.10.
Downloaded from here: https://www.st.com/en/development-tools/stm8cubemx.html
From the manual found here: https://www.st.com/resource/en/user_manual/um2125-stm8-configuration-tool-stmicroelectronics.pdf :
[to install]On Linux:
a. Make sure you have access rights to the target installation directory. You can run the installation as root
(or sudo) to install STM8CubeMX in shared directories.
b. Double-click (or launch from the console window) on the SetupSTM8CubeMX-VERSION.linux file.
Double clicking on the file has no effect. Running from terminal doesn't work either..
jason@Jason-Desktop:~/Downloads/STM8$ dir
Readme.html SetupSTM8CubeMX-1.5.0.app SetupSTM8CubeMX-1.5.0.exe SetupSTM8CubeMX-1.5.0.linux
jason@Jason-Desktop:~/Downloads/STM8$ sudo ./SetupSTM8CubeMX-1.5.0.linux
sudo: unable to execute ./SetupSTM8CubeMX-1.5.0.linux: No such file or directory
The file (SetupSTM8CubeMX-1.5.0.linux) is executable. Java runtime environment is installed. Ideas?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-01-31 1:15 AM
Hello,
using mainly STM32 MCUs, it happens I'm in need to do some STM8 stuff.
being familiar with STM32CubeMX its kind of obvious to use STM8CubeMX as well, but I run into the same issue.
The problem is, the binary file delivered by ST is a 32-bit executable(even if Readme.html states, "Linux: 64-bit (x64) (tested on RedHat, Ubuntu and Fedora)"), so it doesn't run native on 64-bit OS.
file SetupSTM8CubeMX-1.5.0.linux
SetupSTM8CubeMX-1.5.0.linux: ELF 32-bit LSB executable, Intel 80386, version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux.so.2, for GNU/Linux 2.6.24, BuildID[sha1]=5214e1e4682c839df2c0aab9a9338b649e50e54c, not stripped
I guess ST has to do something about it.