2026-01-07 6:23 AM - edited 2026-01-07 6:27 AM
I'm running Bazzite (Fedora 43) and tried to install STM32CubeMX on a Fedora distrobox and was met with some issues.
First, the installer is unable use /bin/chmod, this is fixed by switching out the installer's `jre\bin` directory for OpenJDK.
Second, if you run as a normal user it fails with:
com.izforge.izpack.api.exception.IzPackException: An error occured in java.lang.Thread.run() at Thread.java:1583 in com.izforge.izpack.installer.unpacker.UnpackerBase.run() at UnpackerBase.java:241 in com.izforge.izpack.installer.unpacker.UnpackerBase.unpack() at UnpackerBase.java:319 Caused by: com.izforge.izpack.api.exception.InstallerException: File execution failed in com.izforge.izpack.installer.unpacker.UnpackerBase.unpack() at UnpackerBase.java:299 in com.izforge.izpack.installer.unpacker.UnpackerBase.unpack() at UnpackerBase.java:483 in com.izforge.izpack.installer.unpacker.UnpackerBase.executeFiles() at UnpackerBase.java:959
This is fixed by running the installer via sudo.
This is what I did to get it running in distrobox:
cd distrobox create --name stm32cubemx distrobox enter stm32cubemx sudo dnf install java-latest-openjdk.x86_64 mv jre jre.st mkdir jre ln -s /usr/bin jre/bin chmod +x SetupSTM32CubeMX-6.16.1 sudo ./SetupSTM32CubeMX-6.16.1
cd /usr/local/STMicroelectronics/STM32Cube/STM32CubeMX/ sudo nano STM32CubeMX.desktop
[Desktop Entry] Version=6.16.1 Name=STM32CubeMX-6.16.1 Comment=STM32CubeMX Application for STM32 development Exec=/usr/local/STMicroelectronics/STM32Cube/STM32CubeMX/STM32CubeMX Icon=stm32cubemx Terminal=false Type=Application Categories=Development;
distrobox-export --app /usr/local/STMicroelectronics/STM32Cube/STM32CubeMX/STM32CubeMX.desktop
With this, I'm able to run 6.16.1, but the MCU selector, board selected and various other progress dialog windows are just empty with a white background. It does load up existing projects however.
Other users report that 6.16 has rendering issues on Fedora 43.
I was able to install CubeMX 6.15 from the Baazar store (flatpak) just fine, and that doesn't have any issues rendering the MCU selector or other dialog windows.
2026-01-07 6:44 AM
Hello @DClif.1
Based on RN0094 : 1.2 Host PC system requirements, Fedora 43 is not yet supported with STM32CubeMX.
Below are the supported operating systems and architectures for CubeMX 6.16.1:
• Windows® 10 and 11, 64 bits (x64)(b)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 42(c) (d) (e)
• macOS® 15 (Sequoia), macOS® 26 (Tahoe)(f)
KR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-08 3:45 AM - edited 2026-01-08 3:46 AM
Yes, I became aware of the Fedora 43 limitation.
However, related to this, I tried using 6.15.0 via distrobox and had no installer errors, but still had the same missing window content issues as 6.16.1 did. that is: every pop-up window was empty - window frame, but with no content and just a white background.
flathub has a version of CubeMX, but it is out of date, the version there is 6.15.0 - https://flathub.org/en/apps/com.st.STM32CubeMX
Can you could pass on my experience to the developers so that these issues can be fixed in a future version, or do I need to open a ticket somewhere?
2026-01-10 8:57 PM
I just installed version 6.16.1 of STM32CubeMX without any issues. I just downloaded stm32cubemx-lin-v6-16-1.zip and entered the following commands to install it:
$ unzip stm32cubemx-lin-v6-16-1.zip
$ sudo ./SetupSTM32CubeMX-6.16.1
Run STM32CubeMX with the following command:
$ /usr/local/STMicroelectronics/STM32Cube/STM32CubeMX/STM32CubeMX
Root permissions were needed for installation, but not execution.
2026-01-12 2:43 AM
That procedure does not work on immutable/atomic Linux distributions like Bazzite or Atomic Fedora becuase `/` is read-only, thus some form of container (like distrobox / flatpak) is required instead.
2026-04-21 12:01 PM
I have just tested this with CubeMX 6.17 and Ubuntu 24.04 in a Distrobox container and it is still broken with blank popup windows. I checked out the Flatpak version and that works great. Looking into how they do it I don't see anything special apart from them installing OpenJDK and not using the bundled JRE.