cancel
Showing results for 
Search instead for 
Did you mean: 

HSI OScillator Accuracy

michele2
Associate
Posted on March 24, 2014 at 10:41

I'm start to using an STM8S105 and i'd like to use the internal HSI oscollator.

Microcontroller datasheet give indication on HSI accuracy using a table where in the worst case with a VDD of 5Vdc we have +/-3% of tolerance maximum in the complete temperature range.

Having a look of the graphics however the tolerance it seems to be greater, till -4% at -40°C.

Moreover the second graphics shows the accuracy for different power supply voltages from 2.9 till 5.5Vdc. Could someone give me an indication about what to consider as worst case without to use any other sw calibration?

thanks in Advance.

regards

 
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0