STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L Discovery USART

Posted on July 03, 2012 at 19:59i want to transmit using the stm8l152 on the stm8l discovery board. For that i have used sys config registers to remap the clk and the tx pin to the Port A. I use stvd and raisonance compiler. i cannot understand why ...

Compilation Issue

Posted on January 09, 2014 at 13:32There's an error which occurs quite commonly:  proj_name.lkfsymbol_f_NonHandled_Interrupt multiply defined in stm8l15x_it.o  While searching for the above string, there ain't any multiple definition for the same, a...

ST-LINK/V2 not seeng MCU

Posted on July 12, 2012 at 20:08Device: ST-LINK/V2 with firmware V2.J15.S4MCU: STM8L101K3T6i'm trying to connect MCU through the SWIM  in ST visual programmer but always getting ''Check the SWIM cable connection and check all the needed pin connecti...

khorght by Associate II
  • 1586 Views
  • 4 replies
  • 0 kudos

Disable pull down on MISO

Posted on January 10, 2014 at 11:01Hello,I want to disable the pull down of the internal SPI module, as I use the external slave pull down, is there a way to do it?EDIT:The MISO is driven only when NSS is released, handling NSS through software disa...

Debug (printf)

Posted on May 29, 2013 at 13:40Hi all, Just a little question about ST VD and STM8. Is it possible to use the ''printf'' or ''putchar'' functions in debug mode to display a message in a console or something like that ? (I mean without using USART) I...

ST-Link/V2 Programming Issue

Posted on September 06, 2013 at 12:39I am trying to load program using STVD (ST-Link/V2) but getting the error ''can't communicate with the device''. I am only applying Vcc and Gnd to controller + 4 wires of SWIM cable. What should I do? Do I need t...

harsh by Associate II
  • 926 Views
  • 2 replies
  • 0 kudos

STM8L152C6T6 - PWM output compare

Posted on December 17, 2013 at 01:26Hi everyone,I need to generate a square wave and I've written some code but it doesn't work as i want. Can anyone help me with my doubts please?first of all: I'm not sure that the following registers are in hexade...

gibba by Associate II
  • 612 Views
  • 1 replies
  • 0 kudos

STM8L152C6T6 - frequency counter

Posted on December 16, 2013 at 00:23Hi everyone,I'm working on a frequency counter and I'd like to use the internal timers of the mcu. Do some application notes exist related to this topic? I couldn't find any link. Otherwise, do anyone of you have ...

gibba by Associate II
  • 916 Views
  • 2 replies
  • 0 kudos

Software reset (cold reboot)

Posted on November 15, 2013 at 18:36Hi, I'm looking for the proper (standard?) way for cold rebooting an STM8. I see that the first interrupt handler in the interrupt vector is what is called on startup. With my COSMIC compiler, the name of that fun...

shabbyx by Associate II
  • 2919 Views
  • 2 replies
  • 0 kudos