2012-03-04 06:59 PM
If it's possible to use LSE as the clock source of TIM1 or TIM2/3/5 or TIM4 ?
Use LSE as external trigger of TIM1 or TIM2/3/5 or TIM4 is accepted too, if possible please share some code sample. #stm8-timer-lse2012-03-13 05:43 AM
TIM2_TRIGLSE in
STM8L15x standard peripheral library 1.5.1
Hope this will help. Reagrds,2012-03-19 05:57 AM
Hi,
Ive been searching informations about this subject for a while and I found out that LSE isn't able to be used as clock source for TIM1, but is possible for TIM2 and TIM3 as far as I have found so far. As it is said, also there is an example explaining how to do that in STM Library examples..