2012-03-14 9:57 PM
I'm trying to get I2C working, I've verified I can manually toggle the pins at 400KHz with a pull up resistor. I can't seem to get the I2C code to work correctly though.
input_clock = CLK_GetClockFreq()/1000000;
I2C_DeInit(); I2C_Cmd(ENABLE); I2C_Init(I2C_MAX_STANDARD_FREQ, 0xA0, I2C_DUTYCYCLE_2, I2C_ACK_CURR, I2C_ADDMODE_7BIT, input_clock); (void)I2C->SR1; (void)I2C->SR3; while (1) { while (I2C_GetFlagStatus(I2C_FLAG_BUSBUSY)); I2C_GenerateSTART(ENABLE); while (!I2C_CheckEvent(I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(0xA0, I2C_DIRECTION_TX); while (!I2C_CheckEvent(I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); I2C_SendData(0xCA); while (!I2C_CheckEvent(I2C_EVENT_MASTER_BYTE_TRANSMITTED)); I2C_GenerateSTOP(ENABLE); } The code always get stuck at ''while (I2C_GetFlagStatus(I2C_FLAG_BUSBUSY));
'' I've read the errata and don't really see anything similar to this. Also I currently don't have pull-up resistors on the lines while using this code, would this cause the I2C code to error out and always say its busy? #i2c-busy-bit-set