cancel
Showing results for 
Search instead for 
Did you mean: 

Hi All, what compiler should i use?

leoren_tm
Associate II
Posted on August 17, 2010 at 04:07

Hi All, what compiler should i use?

#stm8-compilers #compiler #raisonance #cosmic #iar

13 REPLIES 13
lowpowermcu
Associate II
Posted on May 17, 2011 at 15:10

Good luck :)

disirio2
Senior
Posted on May 17, 2011 at 15:10

Just a note,

Starting from version 2.1.4 ChibiOS/RT includes support for the STM8L family. A demo for the STM8L-Discovery is also included.

Giovanni

---

http://chibios.sourceforge.net/dokuwiki/doku.php

jeantil88
Associate II
Posted on October 01, 2015 at 13:08

Hello Stefan,

I would like to try the Cosmic compiler with Eclipse. I have managed to built the project according the steps you wrote. But I am not able to flash the device with error:

C:\Cosmic\gmake.exe: Nothing to be done for `flash'.

Where exactly shall I write the lines ''flash : ...'' into the makefile?

Debug  is described quite briefly - would it be possible to write more detailed description of debug configuration?

I want to stop using STVD because of debug - it is enormously slow and whole IDE needs restart after several debuggings. Therefore possibility of debugging in Eclipse is very interesting for me.

Thank you a lot in advance.

Tony

Philipp Krause
Senior II
Posted on October 04, 2015 at 14:26

How about updating that comparison. It currently doesn't even mention the IMO best two compilers for the STM8.

Philipp