2015-04-21 8:15 PM
Hello everyone!
I am using STM8S105 and I don't understand the Illegal Opcode Reset function yet. How does it work? What is its function exactly? And which case do we use it? Thanks and best regards!2015-04-23 5:57 AM
Hello,
There is a small paragraph in the STM8 Reference Manual under the Resets section that talks about the illegal opcode reset. In short any opcode that is executed from the flash or ram that is unknown, i.e. not part of the supported opcodes will cause the microcontroller to reset itself, probably setting a flag in a status register somewhere to indicate the cause of the reset. Obviously one doesn't want the microcontroller executing non valid opcodes as this is likely to cause the software to fault. Hope that helps. Thanks, Ian