2021-10-21 01:46 AM
Hello,
I would like to program an STM8 with the STLINK-V3. The jumpers are set as in the manual. When you plug in the USB cable, there are two text folders.
1. DETAILS.TXT -> Version: V3J7M2B4S1 Build: May 13 2020 17:07:49
2. FAIL.TXT -> The interface firmware FAILED to reset / stop the target MCU
What does the "FAIL.TXT" file mean?
It works with the STLINK-V2, but programming does not work with the STLINK-V3.Hello,
I would like to program an STM8 with the STLINK-V3. The jumpers are set as in the manual. When you plug in the USB cable, there are two text folders.
1. DETAILS.TXT -> Version: V3J7M2B4S1 Build: May 13 2020 17:07:49
2. FAIL.TXT -> The interface firmware FAILED to reset / stop the target MCU
What does the "FAIL.TXT" file mean?
It works with the STLINK-V2, but programming does not work with the STLINK-V3.
2021-12-21 10:40 AM
In case you are not using stm8flash: Check if it works with stm8flash, so you know if your problem is on the host software (whatever you use now) side vs. the STLINK-V3 hardware.
https://github.com/vdudouyt/stm8flash
In case you are already using stm8flash: try if it works with other software (e.g. OpenOCD), so you know if your problem is on the host software (stm8flash) side vs. the STLINK-V3 hardware.