2017-11-17 05:08 AM
Hello,
i'm searching for the Source Code of the EVAL Board STEVAL-ILD004V2 with STM8S103F2 Controller?
I can only found the compiled Firmware.
Can anybody help me?
Best Regards,
Stefan
#steval-ild004v2-source-code?2017-11-17 08:02 AM
Where code is unavailable it generally means there are licensing, export or NDA issues, you should contain your local sales office or FAE to obtain access.
2017-12-05 05:02 AM
Hi Clive One,
thanks for your answer.
Now I put the board into operation but it does not work.
Can it be that the STM8S103F2 is not yet programmed?
Will the board be delivered unprogrammed?
The onboard Led is always dark.
What can i do?
2018-04-12 12:00 AM
We are also looking for the source code. No support from the local ST reps here in Shanghai, been calling several times but nobody picks up.
2018-04-12 01:40 AM
Hello,
The user can download the firmware .hex or .s19 file from the below given link.
STSW-ILD004FW
2018-04-12 01:49 AM
Hello,
I think you can create a account on my.st.com and request for the complete firmware.
2018-04-12 08:49 PM
Yes, I have created the account but don't see anywhere to reach out to ST other than this forum. We called all the listed numbers in Shanghai and they were not helpful at all. The receptionist says we need to give her the name of our contact and since we don't have one so we're stuck. The engineer will go to their office and see if anyone can help today. This is dragging on too long.
2019-01-13 11:09 PM
Hi,
I am looking for the source code also.
Is this one a compiled firmware or this can be modified using the IDE?
Regards,
Walter