2010-12-23 7:48 AM
Holiday greetings!
I am attempting to build an 'ST Assembler Linker' project using ST Visual Develop 4.2.0. Build process seems to work until the obsend step. See build output below:----------- Project coloreffect - ST Assembler Linker - Configuration Debug -------------
Running ST linker
lyn Debug\mapping.obj+Debug\stm8s105c_s.obj+Debug\main.obj, Debug\coloreffect.cod, ;
STMicroelectronics - Linker - rel 3.19
200K namespace for approx 8150 publics
** No Errors found on Link.
obsend Debug\coloreffect.cod,f,Debug\coloreffect .s19.s19,s
At this point it stops. Appears the obsend command has been generated incorrectly. If I enter this command into a dos window, it appears to be waiting for operator input. Portion of exported makefile file below: coloreffect.s19 : $(OutputPath)\mapping.obj $(OutputPath)\stm8s105c_s.obj $(OutputPath)\main.obj $(ToolsetBin)\lyn $(ObjectFiles), $(OutputPath)\$(TargetSName).cod, ; $(ToolsetBin)\obsend $(OutputPath)\$(TargetSName).cod,f,$(OutputPath)\$(TargetSName) .s19.s19,s $(ToolsetBin)\abslist $(OutputPath)\mapping.lsr -exe $(OutputPath)\coloreffect.s19 $(ToolsetBin)\abslist $(OutputPath)\stm8s105c_s.lsr -exe $(OutputPath)\coloreffect.s19 I can correctly build the project by running a bat file with the correct obsend command. The error is also visible in the Project Settings/ST Link tab/Obsend step. Is there some way I can correct this? thx... #obsend-make-assembler-linker-visual-develop2011-03-07 8:59 AM
Hi
Did you find a solution as I have the same problem Re Brian