2009-08-20 04:55 AM
Debugging the demo touch key control software
2011-05-17 06:04 AM
2011-05-17 06:04 AM
Hi,
I am trying to debug the demo touch key control on the evoluation board. I am facing problem to debug it, as i am using only free version tools (cosmic and raisonance. The limitation of the free version is 16K byte flash. Touch key control evoluation code is only 11k bytes of flash. so i was hoping to debug it using my free toolset. But as i have to select stm8s207k6 to start debugging which is having 32k flash. my compiler gives an error. Isnt it possible to debug the evoluation software on evoluation board which has stm8s207k6 with free license. it helps to understand the code flow and lessens the debugging time. regards, Vaibhav. :-[ :-[2011-05-17 06:04 AM
2011-05-17 06:04 AM
2011-05-17 06:04 AM
Thanks Luca for the help,
with your inputs i could able to build the touch control evaluation software but my debugger is still not working. I am attaching a error log gerenated by STVD tool. Please let me know if this is beacause of limited 16k byte free version? where can i check the error description with error logs? Vaibhav2011-05-17 06:04 AM
2011-05-17 06:04 AM
Where can I find the error decription for swim prog error [42004]??
Regards, Vaibhav