cancel
Showing results for 
Search instead for 
Did you mean: 

COSMIC stm8_32k compiler uninstall and install

Egon Boormans
Associate
Posted on November 30, 2017 at 15:53

I just uninstalled and newly installed the COSMIC stm8_32k compiler and applied for a new license, placed the newly received license in the License subfolder but I'm still getting the following error '#error cpstm8 C:\Program Files (x86)\COSMIC\CXSTM8_32K\Hstm8\modsl0.h:1 FlexLM No such feature exists.' I'm also not getting option to select the HKEY_CURRENT_USER or HKEY_LOCAL_MACHINE during installation. Anybody any idea? 

2 REPLIES 2
luca239955_stm1_st
Senior II
Posted on November 30, 2017 at 20:01

Hello,

the stm8_32k compiler is old and is no more supported.

It has been replaced by the FSE version that has no limitations at all: you can doanload it

http://cosmicsoftware.com/download_stm8_free.php

Regards,

Luca

Posted on December 05, 2017 at 15:20

Thanks Luca,

that solved the problem.

Regards Egon.