2017-12-01 2:36 AM
Hi,
I nedd to execute an adc conversion in STM8S003. I read that te conversion time is about 2.3us, but I see that the time in my project is about 25us.
Configuration of CLK_Config(void)
{ /* Initialization of the clock */ /* Clock divider to HSI/1 */ CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);}
Configuration of adc
void ADC1_setup(void)
{ ADC1_DeInit(); ADC1_Init(ADC1_CONVERSIONMODE_SINGLE, ADC1_CHANNEL_1,//ADC1_CHANNEL_0, ADC1_PRESSEL_FCPU_D2, ADC1_EXTTRIG_GPIO, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL1, DISABLE); ADC1_Cmd(ENABLE);}Clock oscillator is internal at 16Mhz
Someone can tell me where are the errors?
Thanks!