2020-10-19 1:32 AM
Hi We have a product in market which uses UPSD3234 controller.
Can someone please suggest a controller that can be used to replace this with minimal code changes that supports
Thank you.
Solved! Go to Solution.
2020-10-19 2:15 AM
This will be almost impossible due to your requirement of "minimal code changes": the UPSD3234 was a 8032 based MCU, which is completely different from the microcontrollers currently provided by STMicroelectronics (STM8/STM32/etc).
Of course you can start a new project that has the same behavior as the one with the UPSD3234, but an STM8 does not offer any USB functionality. You should therefore select a device from the STM32 family, e.g. the STM32F407.
Good luck!
/Peter
2020-10-19 2:15 AM
This will be almost impossible due to your requirement of "minimal code changes": the UPSD3234 was a 8032 based MCU, which is completely different from the microcontrollers currently provided by STMicroelectronics (STM8/STM32/etc).
Of course you can start a new project that has the same behavior as the one with the UPSD3234, but an STM8 does not offer any USB functionality. You should therefore select a device from the STM32 family, e.g. the STM32F407.
Good luck!
/Peter
2020-10-19 2:18 AM
Thank you. We will look into the STM32 series.