2009-11-16 04:23 AM
Compiler question
2011-05-17 06:05 AM
Hi everybody
I´m new here, I am doing a project with a PIC and as I am running out of memory I must change my microcontroller. I have searched a lot and I have decided that my best option is a STM8S207xx, probably C8 or R8. I ask for help with the choice of compiler, I´ve seen that there are two free options, cosmic and raisonance but I think both are limited to 16k of code, is it true?. I need to compile bigger code, so what can I do? I search for cosmic and seems not to be nothing and the raisonance option costs too much for me, is there any other option? and technically, what is considered the best compiler? Thank you very much, best whises! P.D. sorry for my english :-? [ This message was edited by: a.roncal on 06-11-2009 13:11 ]2011-05-17 06:05 AM
Quote:
... I search for cosmic and seems not to be nothing ... Regards, Luca (Cosmic)2011-05-17 06:05 AM
but with this I can compile a code larger than 16 k?
2011-05-17 06:05 AM
Hi,
You will have to buy a Compiler for projects larger than 16KB of code. This is true for both Raisonance and Cosmic compilers. You can check out our Compiler features from Regards, Bruno