2016-02-25 06:20 PM
Hi,
I'm trying to use the Cosmic 32K compiler in ST Visual develop and having created a completely new project with no additional code in, I can't compile it. I can't compile using Idea either.My error is:&sharperror cpstm8 C:\Program Files (x86)\COSMIC\32K_Compilers\CXSTM8\Hstm8\mods0.h:1 FlexLM No such feature exists.main.c: The command: ''cxstm8 +debug -pxp -no -l +mods0 -pp -i''C:\Program Files (x86)\COSMIC\32K_Compilers\CXSTM8\Hstm8'' -clDebug\ -coDebug\ main.c '' has failed, the returned value is: 1exit code=1.Could anybody advise me on how to solve this?Thanks, #stvd-cosmic-compiler-stm8l2016-06-07 11:44 PM
Did you set the toolset root path in the STVP project?
You can find this in the Project Settings -> General tab -> Toolset info -> Tick the checkbox for ''Project specific toolset path''. Then in the box below will be activated where you can provide the path for installation folder of Cosmic compiler.Good luck !2016-10-05 06:05 AM
Hi Ritesh,
After re-requesting the license, all is well now! Thank you for your response.