cancel
Showing results for 
Search instead for 
Did you mean: 

Can the STM8AF series be programmed via the LIN bus using the Flash Loader Demonstrator?

JAYLOU
Associate

Hello community

Can the STM8AF series be programmed via the LIN bus using the Flash Loader Demonstrator?

4 REPLIES 4
AA1
Senior III

I think Flash Loader Demonstrator only supports UART/RS232. But you can try to use LIN. Also you can create your own bootloader.

JAYLOU
Associate

But I only have the lin interface outside of the ecu.

Then someone didn't think the design through very well..

Your own code may have significantly more flexibility in what you can implement, but the ROM based loader have very limited and specific functionality. Initial programming will need to be done via the SWIM interface methods.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AA1
Senior III

I am not familiar with LIN. But UM0560 - STM8 bootloader speaks about LINUART/UART. So your PC need to have a card with LIN interface.