Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.
hi friends i asked my question just a few days ago but nobody answerd i dont know what should i do when i configure micro controller for cco output it generates out put of course its a little unaccurate when i check that is cco stable by checking CCO...
Cosmo has no space limited version, you can download it there, thank you!
I created a program on STM8S103F3 to generate a delay in rage of micro seconds using TIM2 module, but the timer is not ticking as expected and when I tried to call 1 sec delay using it, it is giving around 10 sec delay. I'm using 16MHz HSI oscillator...
Here I am using the STM8s003k mcu .In my application,I am configuring the external interrupts for a port .after rising the interrupt how can I clear that interrupt.If I can not clear that interrupt the external interrupt handler only will execute. I ...
Hi,Reset is not happening at only particular project while debugging using STVD. But the same code is working fine if I load the code through STVP. Same MCU Reset is working fine with other project while debugging. I don't know is there any settings...
Hello,I have got an industrial PCB with a STM8S207RBT6. I'm able to READ programm memory, data memory and option bytes with ST Visual Programmer and STLink V2.Also I can write data memory and option bytes. But if I try to write program memory I get a...
i tested it with below code and ieven change prescalers for lower and higher frequency , i also check it with external crystal (and change the code) but it remains in while(CLK_GetFlagStatus(CLK_FLAG_CCORDY) == FALSE);for ever . when i debug the cod...