STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S power (current) consumtion problem

I'm developing some applications with STM8S003K3 now (battery-used product). The problem is that, I cannot make the MCU consume just 4.5 micro-ampere order current in the halt mode as in the datasheet described.I use the Eval-Board "STM8SVLDISCOVERY"...

MBern.5 by Associate
  • 1124 Views
  • 2 replies
  • 0 kudos

Not able to get license Key of Cosmic C compiler

Hi i am starting firmware development on STM8 based MCU. For that in need Cosmic C compiler but after its installation , for generating the key when i choose option "on the web"it does not send any mail to my registered Email address and if i choose ...

KGupt.1 by Associate III
  • 1360 Views
  • 1 replies
  • 0 kudos

STM8S001j3 SWIM Pin lock, How to do Firmware level

STM8S001j3   SWIM PIN Not work, After hex file download (IAR EWSTM8 Compiler)8 pin port (SWIM) How to do in the firmware IAR.-DATASHEET 12page-Recommendation for SWIM pin (pin #8) sharingAs the NRST pin is not available on this device, if the SWIM...

csocom by Associate II
  • 608 Views
  • 0 replies
  • 1 kudos

can't be complied successfully

Hi , i try to run the CLK example from STM8L15x_StdPeriph_Examples, but i can't compile the project successfully , below is my procedure, can you help it?create a new workspace using STVD tooladd the source and head files from the STM8L15x library f...

ALiu.5 by Associate II
  • 875 Views
  • 3 replies
  • 0 kudos

Alternative Debuggers for STM8

Hi :)So I've been using the lovely software provided by ST, called ST Visual Develop, which is, not only one of the worst IDE I have ever encountered (I quickly switched to writing the actual code in another editor), but also is full of so many bugs....

SLasn.1 by Senior
  • 693 Views
  • 1 replies
  • 0 kudos

Update for STM8 Bootloader Manual (UM0560)...?

the STM8 bootloader manual (UM0560 rev10) appendix B describes fewer families/bootloader versions than the erase/write RAM routines bundled with the FLASHER-STM8 v2.8.0. Specifically the newer BL versions v2.4 and v1.4 are missing, as well as the 256...

GIcki by Associate II
  • 626 Views
  • 0 replies
  • 0 kudos