STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8 and ST-link programming under Linux (Raspberry pi)

Hello,I have to program STM8 device under Raspberry Pi OS. But I can't find any support page explaining how to use ST-Ling under RPI linux. Device is STM8S007C8T6 .It is not necessary that I have to use ST-Link, I only have to connect to and prog...

mladen by Associate II
  • 1760 Views
  • 2 replies
  • 0 kudos

How to overcome adc fluctuation.

Hiii guys, i am using stm8s003f3.i configure it according to datasheet and it work almost fine,but problem is, it is generating random voltage when there is no input is connected and because of this input fluctuation getting unwanted output.how to ma...

MAnsa.1 by Associate II
  • 2018 Views
  • 6 replies
  • 0 kudos

Is it possible to optimize the dlstm8smn.a library?

Hi all, I'm new to developing with the STM8 and noticed that the dlstm8smn.a library is taking up nearly 1kB of flash in my project. I'm wondering if someone could help demystify what all these object files are doing and where I could potentially opt...

0693W000007DLw0QAG.png
Konami by Senior II
  • 618 Views
  • 0 replies
  • 0 kudos

Need STM8L development Guidance

I have posted already that I am using STM8152R8 nucleo board I have downloaded cosmic c compiler and it's license file too. I have also downloaded the STM8L library (en.stsw-stm8016) from the ST website. I have included the source files and include...

DJosh.0 by Associate II
  • 4419 Views
  • 12 replies
  • 0 kudos

stvd project settings panes too big

My stvd project settings panes for Compiler and to the right of it have font size too big. Consequentially I can only acess the top left of the pane. I need to change the const section address and I can't get to it, so my project is on hold until ...

mchahn by Senior
  • 808 Views
  • 3 replies
  • 0 kudos

MCU STM8 as SPI slave

Hello. I want to make the controller a slave for the SPI. I understand the hardware activation Support leg stm8 at present, as it was then activated receiving \ transmitting?/* Includes ----------------------------------------------------------------...

k.s.corp by Associate II
  • 667 Views
  • 0 replies
  • 0 kudos