STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to connect st-link v2 with Tag-connect cable

HiI plan to program my MCU using a Tagconnect cable. I haven't bought the Tagconnect cable yet, nor the st-link v2, and I would like some recommendations.Is anybody using this setup? What are your thoughts?It also seems there are different versions o...

0693W00000Lwl4pQAB.jpg 0693W00000Lwl8lQAB.jpg
lyoy by Associate III
  • 5615 Views
  • 4 replies
  • 0 kudos

Another problem with the problematic STM8L050J3

Hi there,I have made changes to the firmware and , via ST-Link V2, I would like to reprogram an STM8L050J3, which I had previously programmed with the Active Halt function enabled, but SVP does not allow it and responds with this message as the attac...

Resolved! No output from TIM2 in compare mode on STM8L101F3

I am trying to get a pulse out of TIM2 in compare mode but I see no output. Here is my snippet of code:#include "iostm8l101f3.h" void main( void ) { CLK_CKDIVR = 0x01; // 8MHz PA_CR1 = 0xFF; // all pullups PB_DDR = 0x01; // 0000 0001...

AMacd.1 by Senior
  • 1266 Views
  • 1 replies
  • 0 kudos

CLK_AdjustHSICalibrationValue, STVD Error

Hello,I am developing a project with STM8L050J3 microcontroller using Evaluation Board STM8-S08-DISCO and STVD version 4.3.12.I need to calibrate the internal HSI oscillator, but for some reason that I have not been able to identify, although I compi...

Resolved! Unable to write to TIM2 Registers

I have this little project for the STM8L101F3 that just writes an arbitrary value to TIM2_CCR1H and TIM2_CCR1L and then tries to start the timer but I get nothing from the timer output.If I run the project with a debugger and inspect the contents of ...

AMacd.1 by Senior
  • 2554 Views
  • 8 replies
  • 0 kudos

Resolved! How to decode QFN20 marking ?

Hello, there is posibility we mixed STM8L101F3 vs F3U. There is marking L1S3 on the top, but I can't find any information/table of these markings. Is is possible to have it ?