2022-03-09 9:16 PM
Can the TIM1 part of this tutorial be simplified as follows?
https://embedded-lab.com/blog/continuing-stm8-microcontroller-expedition/6/
Remove everything related to the the interrupt, because TIM1_GetCapture2() can be called at any time from main(). It will always contain the last capture duty cycle.
Reduce TIM1_setup(void) to:
TIM1_DeInit();
TIM1_TimeBaseInit(2000, TIM1_COUNTERMODE_UP, 55535, 1);
TIM1_PWMIConfig(TIM1_CHANNEL_1, TIM1_ICPOLARITY_RISING, TIM1_ICSELECTION_DIRECTTI,
.... TIM1_ICPSC_DIV1, 0);
TIM1_SelectInputTrigger(TIM1_TS_TI1FP1);
TIM1_SelectSlaveMode(TIM1_SLAVEMODE_RESET);
TIM1_CCxCmd(TIM1_CHANNEL_1, ENABLE);
TIM1_CCxCmd(TIM1_CHANNEL_2, ENABLE);
TIM1_Cmd(ENABLE);
Because:
The second TIM1_PWMIConfig() is redundant because it simply overwrites the values set in the first call.
Reordered function calls to match the procedure described on page 170 in RM0016 manual.