cancel
Showing results for 
Search instead for 
Did you mean: 

what is the meaning of 'EXTI_IT_Pin7' in the below-given code? I am using the STM8L1526 Discovery Board.

ASing.20
Associate II

#include "stm8l15x.h"

#include "stm8l15x_gpio.h"

#include "stm8l15x_itc.h"

#include "stm8l15x_exti.h"

#include "stm8l15x_clk.h"

#include "stm8l15x_rtc.h"

#include "stm8l15x_tim2.h"

#include "stm8l15x_tim1.h"

#include "stm8l15x_tim3.h"

#include "stm8l15x_tim4.h"

#include "stm8l15x_adc.h"

#include "stm8l15x_pwr.h"

// void Halt_init();

// void GPIO_LowPower_Config(void);

//

void Delay(__IO uint32_t nCount)

{ /* Decrement nCount value */

  while (nCount != 0)

  {

    nCount--;

  }

}

void main()

{

  // Halt_Init();

        TIM1_Cmd(DISABLE);

        TIM2_CtrlPWMOutputs(DISABLE);

        TIM2_Cmd(DISABLE);

        TIM3_Cmd(DISABLE);

        TIM4_Cmd(DISABLE);

        ADC_Cmd(ADC1, DISABLE);

        PWR_PVDCmd(DISABLE);

        /* Switch to LSI as system clock source */

        /* system clock prescaler: 1*/

        CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1);

        CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_LSI);

        CLK_SYSCLKSourceSwitchCmd(ENABLE);

        while (CLK_GetFlagStatus(CLK_FLAG_LSIRDY) == 0);

        CLK_HSICmd(DISABLE);

        CLK_HSEConfig(CLK_HSE_OFF);

        /* Set STM8 in low power */

        PWR_UltraLowPowerCmd(ENABLE);

        /* Set GPIO in low power*/  

        /* Configure unused pins as output push-pull 0 to enter low power */

        /* Port A */

        GPIO_Init(GPIOA, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow);

        /* Port B not AIN */

        GPIO_Init(GPIOB, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);

        /* Port B LEDs, so they don't flash at power on */

        GPIO_Init(GPIOB, GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5, GPIO_Mode_Out_PP_High_Slow);

        /* Port C not wakeup pin!! */

        GPIO_Init(GPIOC, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6, GPIO_Mode_Out_PP_Low_Slow);

        /* Port D */

        GPIO_Init(GPIOD, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow);

        /* Port E */

        GPIO_Init(GPIOE, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow);

            /* Port F */

        GPIO_Init(GPIOF, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow);

        /* Stop RTC Source clock */

        CLK_RTCClockConfig(CLK_RTCCLKSource_Off, CLK_RTCCLKDiv_1);

        /* Stop clock RTC and LCD */    

        CLK_PeripheralClockConfig(CLK_Peripheral_RTC, DISABLE);

        CLK_PeripheralClockConfig(CLK_Peripheral_LCD, DISABLE);

  GPIO_Init(GPIOC, GPIO_Pin_3, GPIO_Mode_Out_PP_Low_Fast);

  GPIO_ToggleBits(GPIOC, GPIO_Pin_3);

  Delay(90000);

  EXTI_ClearITPendingBit(EXTI_IT_Pin7);

  halt();

  GPIO_Init(GPIOE, GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Fast);

  GPIO_ToggleBits(GPIOE, GPIO_Pin_7);

  Delay(90000);

}

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Artur IWANICKI
ST Employee

Hello. This line is clearing one of the bits within EXTI_SR1 register which indicates occurrence of external interrupt on any of pin7 within MCU. In STM8L devices you can configure EXTI interrupts per pin or by port (in this second case EXTI_SR2 register is taken into consideration).

View solution in original post

2 REPLIES 2
Artur IWANICKI
ST Employee

Hello. This line is clearing one of the bits within EXTI_SR1 register which indicates occurrence of external interrupt on any of pin7 within MCU. In STM8L devices you can configure EXTI interrupts per pin or by port (in this second case EXTI_SR2 register is taken into consideration).

Thank you!!