cancel
Showing results for 
Search instead for 
Did you mean: 

Timer as frequency/RPM counter, CapCom offset?

klaasdc
Associate II
Posted on June 13, 2012 at 21:02

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
klaasdc
Associate II
Posted on June 27, 2012 at 21:31

Has no one used a timer to measure input signals?

:(

klaasdc
Associate II
Posted on June 27, 2012 at 22:26

Could it be that the timer misses a few ''counts'' after it is being reset in Slave Mode? (TIM1_SLAVEMODE_RESET)

That would explain why I always end up with frequency values that are too high (or periods that are too low for that matter)....