Skip to main content
mrtaotao789
Associate II
April 5, 2016
Question

[SOLVED] problem with STVD + COSMIC.. STM8S103K + ST-LINK_V2

  • April 5, 2016
  • 1 reply
  • 1222 views
Posted on April 05, 2016 at 15:26

First i'm sorry for my bad in english

i have 2 problem for STVD+COSMIC

/**------------------- 

first question

 -------------------- **/

#include

''stm8s103k.h''

int main(void)

{

CLK_CKDIVR = 0; // prescaler system clock = 1

while( (CLK_ICKR & 2)==0 ); // wait HSI ready

TIM1_ARR = 1600 - 1; // auto reload 100 usec

TIM1_CR1 = 1; // enable timer_1

PB_DDR |= 1<<3; // o/p.. pin_B3

PB_CR1 |= 1<<3; // push_pull

while (1){

if( TIM1_SR1 & 1 ){

TIM1_SR1 &= ~1;

PB_ODR   ^= 1<<3;

}

}

}

This code.. TIM1_CNTR can not over flow by TIM1_ARR's value (1599)

TIM1 counting to 0xFFFF and over flow

But this code can overflow and reload with TIM1_ARR's value (1599 = 0x0639)

Output pulse of ODR_B No3 is 5kHz.. which is valid

(with IAR.. i edit TIM1_ARR to..

   TIM1_ARRH=0x06;

   TIM1_ARRL=0x39;)

What i missing coding..?

/**------------------- 

second question

 -------------------- **/

#include ''stm8s103k.h''

void system_config ( )

{

CLK_CKDIVR = 0;

// prescaler system clock = 1

while( (CLK_ICKR & 2)==0 );

// wait HSI ready

TIM1_ARR

= 1600 - 1;

// auto reload 100 usec

TIM1_CR1

= 1;

// enable timer_1

}

int main(void)

{

system_config ( ) ;

PB_DDR |= 1<<3; // o/p.. pin_B3

PB_CR1 |= 1<<3; // push_pull

while (1){

if( TIM1_SR1 & 1 ){

TIM1_SR1 &= ~1;

PB_ODR   ^= 1<<3;

}

}

}

when rebuild all...

Compiling main.c...

 

cxstm8 -i''c:\program files\stmicroelectronics\st_toolset\include''\

+mods0 +debug -pxp -no -pp -l -i''C:\Program Files\COSMIC\FSE_Compilers\

CXSTM8\Hstm8''  -clDebug\ -coDebug\ main.c

#error cpstm8 main.c:11(15) missing prototype

main.c:

 

 The command: ''cxstm8 -i''c:\program files\stmicroelectronics\

st_toolset\include'' +mods0 +debug -pxp -no -pp -l -i''C:\Program Files\

COSMIC\FSE_Compilers\CXSTM8\Hstm8''  -clDebug\ -coDebug\

main.c'' has failed, the returned value is: 1

exit

code=1.

line : system_config() in  main(void)

But this code can complier and debug in IAR_for_STM8

with output pulse 5kHz ODR_B3

How do i solve this problem

i am very confuse.  @_@!

Thank you very much for answer.

Sorry for my bad in English again

^_^!

/*******************************************/

Now i can solve this problem

Thank you 

Liem HUA.. of 

htl@cosmic.fr

2-way for fix :

1. remove -pp option of complier of STVD

tab : Project -> Setting -> C_Complier -> C_Language

Change_setting from Enforce_Function_Prototyping -> Default

2. change Prototype(){ /* code */ } .. (old of my)

   to     

Prototype(void){ /* code*/ }

^_^!
    This topic has been closed for replies.

    1 reply

    wangyx2012
    Visitor II
    April 6, 2016
    Posted on April 06, 2016 at 08:33

    check TIM1_CR1 ARPE bit,please!